10/18/2014 6:00 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308) |
Hello gordon2014 Motion Controlwas only a part of the SIMADYN-D portfolio. In that respect, certainly we have very good solutions in the form of SIMOTION or integrated Motion Control. But these at best replace T400 module. We use FM458 + EXM338 for High speed Closed Loop controls in Metal Processing among others especially for Highly demanding applications like Automatic Gauge Control etc. This allows us to provide a Dedicated High speed control within a S7-400 system . The High Speed I/Os and Encoder Inputs integrated in EXM338 is ideally suited for such applications. To the best of my knowledge there is no hardware available which even remotely matched the FM458 capabilities. I hope Siemenswill not do away with this excellent piece of hardware. Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on