Industry Online Support
Technical Forum
10/22/2014 4:15 PM | |
Posts: 3 Rating: (0) |
I also need this |
10/30/2014 4:31 PM | |
Joined: 10/11/2006 Last visit: 5/3/2024 Posts: 5832 Rating: (789)
|
Hello, Maybe the Drive Lib can help you to create a Profinet / Profibus communication: http://support.automation.siemens.com/WW/view/de/68034568 If you want to use it then use the manual which is also linked on this page. If you want to create your own communication you can use - for the beginning - an application example which contains usefull PLC data types for different standard telegram: http://support.automation.siemens.com/WW/view/de/82841762 |
With best regards, |
|
Follow us on