Industry Online Support
Technical Forum
11/13/2014 10:53 AM | |
Posts: 13 Rating: (0) |
Hi , we are using LFE1/8851 burner sequential controller. Now days we are facing problem during the startup ( after shutdown) . whiel starting burneris tripping with collective fault/ flame failure/trouble burner motor etc... we are not able to troubleshoot the problem. 1) Is any of the plant is using the same controller kindly reply back , you are also facing the same problem or not??? and what action that you had taken for that?? 2) And my second query. Is it possible to replace the LFE1 controller with some other standard burner controller , which should connect to the PLC for better trouble shooting. Already we are using S7 400 & WINCC for the plant control. Regards, Vijayan R Attachmentn7461e-LFE1.pdf (756 Downloads) |
Follow us on