Industry Online Support
Technical Forum
11/26/2014 11:52 PM | |
Posts: 2 Rating: (0) |
Hi Guys, I have exact same issue but with WinCC 7.3. The Station Configuration Editor is not showning WinCC Appl. and it seems I cannot add it. My machine is running on Win 7 64-bit. And I have another machine which is running on same Win 7 64-bit and WinCC 7.2 and I have no problem with it,WinCC Appl. can be seen onStation Configuration Editor, it is only the machine with WinCC 7.3 that I can't add Wincc Appl. Your thought? Thanks
------------------------- New subject after splitting from Station configuration editor not shown for wincc 7.0 |
Last edited by: Min_Moderator at: 11/27/2014 11:44 AMSplitted Last edited by: RMati at: 11/26/2014 11:54 PM |
|
Follow us on