11/14/2014 9:31 PM | |
Joined: 9/17/2008 Last visit: 9/21/2024 Posts: 12 Rating: (0) |
When creating a new project in S7-Web2PLC, then use Export Symbols, it ens with an error E058 "Configuration download failed *** ERROR E058: Configuration: Closing quotation mark ' is missing." I have attached the log file any idea?
AttachmentWeb2PLC_Log - Notepad.pdf (349 Downloads) |
11/26/2014 5:19 PM | |
Joined: 9/17/2008 Last visit: 9/21/2024 Posts: 12 Rating: (0) |
Hi, not sure if I understood what you meant by chosing a different directory, do you mean for the project location? |
11/26/2014 7:21 PM | |
Joined: 9/17/2008 Last visit: 9/21/2024 Posts: 12 Rating: (0) |
And it works just fine! thanks a lot for the help |
12/3/2014 12:47 PM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
newquestion published by Arunkpmis split to a seperate thread with the subjectWeb2PLC - values are shown as integer. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on