12/8/2014 4:15 PM | |
Posts: 3 Rating: (0) |
hi all. i use step 7 microwin sp9 to make my project (s7-200). HSCOMM for INSYS. it's controlled the ouput 1 by SMS. when output 1 is actived, R( such as motor) start and Q0.0 make a pulse ( 1s on, 1s off) then INSYS send me a SMS ( motor start). in the otherside Q0.0 make 2 pulse ( 1s on, 1s off, 1s on, 1s off) INSYS send SMS ( motor stop). when BT's actived the motor stopimmediately and INSYS send emergency. let's the diagram in the attached file. looking forward to hearing from you. tks all AttachmentDesktop.zip (211 Downloads) |
12/8/2014 4:24 PM | |
Posts: 3 Rating: (0) |
more information |
Follow us on