11/18/2007 7:19 AM | |
Posts: 1 Rating:
|
Please Help, I have Blow Molding machine running with CPU 416-3 DP (two Profibus Networks, critical and standard), this was running great for long time. But now I have the machine running for 20 minutes and then the CPU sees a fault at the DP Slave ID 4 which is a IM151-1 HF (ET200S - 6ES7 151-1BA00-0AB0) thas has like 21 slaves at the rack. The Diagnostic Buffer (attached) always reports the same problem with OB122 and make reference to some address related to the modules attached to this ET200S ID=4. I already changed the ET200S once, I already replaced almost all modules (attached is the Hardware configuration for this machine) attached to this ET200S, replaced the Profibus Connector, replaced the Profibus cable, it is the same PLC Program without any modification and still happening the problem every 15 or 20 minutes. If some body can help me in this, looking the information that I am attaching, I really will appreciate. I am burned out and I can not find a solution for now. Thanks, Racartapo AttachmentBuffer and Program.zip (701 Downloads) |
Follow us on