12/31/2014 12:57 PM | |
Posts: 6 Rating: (0) |
Hello,
I have the problem with the connection via MPI or Profibus.
I have following configuration: Win7 Enterprise SP1 64-bit STEP 7 Professional 2010 SR2
Wenn I go to the Set PG/PC Interface and try to make net diagnostic I got the error: Error 0xe9:Could not start a utility for initialization/synchronization
What is strange, that simultaneously two interfaces are active: MPI and USB-Adapter Profibus
The button “Add/Remove” Interfaces is deactivated. Test shows than the MPI-interface has a problem:
What can I do in this case?
Thanks and Happy New Year!
AttachmentC:\Interface.zip (69 Downloads) |
Last edited by: userdok at: 12/31/2014 1:37 PM |
|
1/8/2015 11:25 AM | |
Posts: 366 Rating: (30) |
In which way you wanna basically go online? What is your hardware? Are you working with USB-Adapter or CP5611 PB-Card? nice regards
|
Follow us on