1/15/2015 7:46 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, there is no successor in S5. You need a S7 F-PLC. You have 2 options. - upgrade to S7 - spare part for S5. there is no 8BFA02 - only8FA02 or 8FB02.I have both types in stock. Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
This contribution was helpful to1 thankful Users |
1/15/2015 9:13 AM | |
Joined: 10/7/2005 Last visit: 5/2/2024 Posts: 3004 Rating: (1046)
|
It seems there's some confusion going on here, so lets see what Siemens themselves have to say about this: The 6ES5095-8FA02 was discontinued in 2007 (but by doing a search on the web willfind a fair few sources to get this one from). It's successor is the 6ES5095-8FB01whichwill be discontinued in 2020, so youmay still be able to get it. So much for the good news. You are dealing with a Safety S5 95U and are best advised to read up on the available manuals first which will also tell you if you can re-use the EPROM(and may need to replaceboth CPU's together). |
Cheers |
|
This contribution was helpful to1 thankful Users |
1/16/2015 1:53 AM | |
Posts: 2 Rating: (0) |
Thanks for your valuable info, will work on that! |
Follow us on