2/13/2015 8:27 AM | |
Posts: 41 Rating: (1) |
Hi All I'm looking for a copy of PCS7 V6.0 SP1. Is there somewhere where I can download it. |
2/13/2015 1:57 PM | |
Posts: 46 Rating: (3) |
Unfortunately there is no such a possibility of a download. PCS 7 is provided on DVD only. |
2/16/2015 8:32 AM | |
Posts: 32 Rating: (4) |
Hi Tuff, unfortunately there is no official download for the PCS 7 V6.0 SP1 because this version is in the end of production > https://support.industry.siemens.com/cs/ww/en/view/67267478 But when you want it at all costs you can create a support request It will cost you a bit but there you get a download link for the PCS 7 V6.0 SP1 Regards |
Follow us on