2/19/2015 2:16 PM | |
Posts: 74 Rating: (0) |
Would it be possible to provide me with an example of the alarm flip flop in FBD, I am confused as to what you mean |
2/19/2015 2:30 PM | |
Posts: 74 Rating: (0) |
Hi I have attached a screenshot of my Flip flop, I cannot upload a file of the alarm management as I don't know how to generate it AttachmentAlarm1.zip (112 Downloads) |
2/19/2015 6:56 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Don't use an input for flip-flop address.In my case, M10.0 used to keep the alarm.Also , it is possible to keep all alarms in a DB.To generate alarm, use this address.Do you use SIMATIC WinCC or WinCC flexible? Attachment1.zip (86 Downloads) |
2/20/2015 10:29 AM | |
Posts: 74 Rating: (0) |
I am using WinCC flexible but its been integrated into my SIMATIC manager. regards Jimbo |
2/20/2015 10:33 AM | |
Posts: 74 Rating: (0) |
From your example, is the Set input to the flip flop the BOOL in my case the switch? regards Jimbo |
3/2/2015 7:36 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Just to increase your chance to get an answer, please start a new thread in WinCC Flexible conference (or any related) .I can only say that panels are not very good for tag logging.As a starting point, please check the following FAQ and see if it helps: How can you have data from a tag log displayed in table form for panels or the WinCC flexible PC Runtime? |
Follow us on