2/19/2015 5:25 PM | |
Posts: 9 Rating: (0) |
Hello All,
I have a hardware config in a PLC program I am unable to change if I need to in the future. There is a CP343-1 Advanced IT in the hardware config that my PG will not recognize. I have tried installing the updates and hot fixes per the CD that came with the CP343-1 Advanced IT and searched on line. So far I am having no luck. The required hardware update shows up in the hardware config when I want to install updates, but after installing the updates the CP343-1 Advanced IT update will give a message saying it could not be installed.
Attached is all the information I have with several screen shots.
Any ideas?
If anyone needs more info let me know. Hopefully it is something simple I am doing / not doing that can someone can point out.
Thanks,
Larry
AttachmentPG_problem_CP343.pdf (58 Downloads) |
2/20/2015 8:11 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
[quote] Configuration software ● required STEP7 V5.5 SP2 HF1 or higher / STEP 7 Professional V12 (TIA Portal) or higher ● for PROFINET CBA / required SIMATIC iMap V3.0 SP4 and higher [/quote] Yes, you have the version but try it with update the Step7 to SP4 (http://support.automation.siemens.com/WW/view/de/93842624)... |
2/20/2015 9:58 PM | |
Posts: 9 Rating: (0) |
Umencho, Thank you for the reply. I downloaded and installed SP4, but now the hardware update for the CP343 (6GK& 343-1GX31-0XE0, HWupdate#1058) does not show up as a HWupdate. I have verified that the update (1058) is located on the hard drive in the default location (see attached). I was able to locate the CP343 part number in the tree, but it is located under I/O. Any ideas why the update is not visible? Thanks, Larry AttachmentPG_problem_CP343_after_install_SP4.pdf (46 Downloads) |
Follow us on