12/2/2007 5:03 AM | |
Posts: 65 Rating: (0) |
So I have to add ladder in the CPU to tell it what tags to read/write ? |
12/3/2007 3:12 AM | |
Posts: 65 Rating: (0) |
I'm having difficulty in even turning on an M address bit using a button in the HMI. |
12/3/2007 8:56 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Please make the merker you want in the symbolic and give it a name, when you look after that with WinCC Flexible into the variables then you may have your answer. There are also getting started for WinCC Flexible with a software example: WinCC flexible Getting Started First Time User WinCC flexible Getting Started Power User WinCC flexible Getting Started Options Look especially to the "Info" to the right of the download |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on