3/11/2015 10:50 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
It can be both. In case of MDS D400: |
3/12/2015 5:11 AM | |
Posts: 10 Rating: (0) |
If starting 2000 bytes reserved for user memory then if we put MDS address 16#0 then it should be read and write properly. "//Commonds MOBY" "MOBY_CMD".CH_I[1].command=02(forwrite=1) "MOBY_CMD".CH_I[1].sub_command=0 "MOBY_CMD".CH_I[1].length=10 "MOBY_CMD".CH_I[1].address_MDS=16#0 "MOBY_CMD".CH_I[1].DAT_DB_address=0 "MOBY_CMD".CH_I[1].DAT_DB_number=1102 But issue is when give command for write the ready signal goes low(writing start) and after write completed again high. at same time if we give read command nothing changes and there is no error in both cases. is it writing properly? is it required configuration of Tag? AttachmentMOBY_DB.pdf (603 Downloads) |
Last edited by: sk800406 at: 3/12/2015 6:29:37 AM |
|
Follow us on