4/10/2015 2:13 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello waran2014, If you have a redundant Serverpair with WinCC V7.2, the Master "makes" the Alarmlogging and send it to the StandBy-PC. You should not get such effects, without the Redundancy does not really, and one or both computers running as "Standalone". You should check the value of the internal Tag "@RedundantServerState" on both PCs. 1 means Master, 2 means StandBy, 3 means Fault and 4 means StandAlone. I do not think, that this FAQ solve the behaviour: Regards Georg Berrghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
Follow us on