5/6/2015 7:59 AM | |
Posts: 5225 Rating: (1192) |
My confusion now comes in with your word of "standard". "Standard" access is where you can see the addresses.. not optimised. I do not see any other option than switching over to symbolic addressing on the library functions that you have.. unless there is no bit orientated variables.. then you should be able to guess. The good thing about using symbolic addressing is that there is a high possibility that your program stays the same even if the library function change a little. Else.. [LINK] w |
5/6/2015 9:23 AM | |
Posts: 5225 Rating: (1192) |
Hi. Please see the attached PDF.
Search for the following phrases in the in-software help: "Blocks with optimized access" "Basics of block access" "Setting up block access" Also you can consult the Step7 documentation.. STEP 7 Professional V13.0, Star worthy? (wink) (smile) AttachmentBasics on block access.pdf (1949 Downloads) |
This contribution was helpful to2 thankful Users |
5/6/2015 9:33 AM | |
Joined: 11/8/2011 Last visit: 9/19/2023 Posts: 89 Rating: (1) |
Yes, 5 star worthy ;). Thank you for the details. BR, h2_504 |
This contribution was helpful to2 thankful Users |
Follow us on