5/18/2015 6:46 AM | |
Joined: 8/25/2006 Last visit: 6/4/2024 Posts: 2206 Rating: (278) |
Hello. Terminal X177:12 (DI1) is used as ON/OFF1, X177:13 (DI2) is used as ENABLE. You can read about these commands in the manual, chapter 10.9. Also look at List manual, funct diagrams. X177:11 is free digital input. By default, analog input X177:25,26 (AI0) is used as main speed setpoint. |
This contribution was helpful to1 thankful Users |
5/18/2015 5:35 PM | |
Posts: 4 Rating: (0) |
Thank you, I will read the chapter and test the drive. |
Follow us on