7/30/2013 1:12 PM | |
Joined: 10/11/2006 Last visit: 7/10/2024 Posts: 5872 Rating:
|
Hello, very helpful for motor dimensioning is the tool Sizer. http://support.automation.siemens.com/WW/view/de/54992004 Otherwise you can check your rated points with a configuration manual. Especially for your case, Asynchronous motor, you could check a 1PH8 motor. Download config. manual: http://support.automation.siemens.com/WW/view/de/46484744/0/en E.g. Prated = 18 Kw speed = 1500 Rpm
1PH8135-1xF with the rated point 18,5KW @ 1500rpm The motor is very flexible so you can select various of encoder, bearings etc. Please control with the config. manual. The 1PH8 is a Asynchronous-Servo-Motor. For less requirement you could also use a 1LE1 motor. It's a standard Asynchronus motor. |
Last edited by: TechTeam at: 7/30/2013 1:16 PMWith best regards, |
|
5/26/2015 2:34 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
|
Follow us on