5/28/2015 9:43 AM | |
Joined: 6/1/2009 Last visit: 1/4/2023 Posts: 27 Rating: (0) |
yes i tried and result is same |
S.H.O |
|
5/28/2015 11:57 AM | |
Joined: 6/1/2009 Last visit: 1/4/2023 Posts: 27 Rating: (0) |
versions of Step 7- 5.4+sp5, CFC v6.1 and D7-SYS 6.2 order number of FM458 - 6DD1607-0AA0
|
S.H.O |
|
5/28/2015 12:14 PM | |
Joined: 8/25/2006 Last visit: 5/15/2024 Posts: 2205 Rating: (277)
|
There is a problem of DUST1 installation in Step 7 V5.4 SP3 + D7-SYS V6.2, may be this also affects on MPI interface. I think in your case (Step 7 V5.4+SP5) there may be the same problem. Basically this combination is not compatible. You need at least D7-SYS V6.2 SP3 HF3 or higher. SP3 you can download here, also you will need SP1 for CFC V6.1. For HF3 (or higher) for D7-SYS V6.2 SP3 you must create Support request. |
5/29/2015 9:52 AM | |
Joined: 6/1/2009 Last visit: 1/4/2023 Posts: 27 Rating: (0) |
Hi ksn I updated cfc v7.1 and d7-sys v7.0 and try again.the result is same. I mean in the load page online and initial chekbox is deactive. in load page when just interface dust1 choosed ,"online and initial " was active. thanks for replys. AttachmentCamera.rar (203 Downloads) |
S.H.O |
|
Follow us on