7/8/2015 4:36 AM | |
Joined: 1/25/2015 Last visit: 4/21/2022 Posts: 22 Rating: (0) |
Dear Expert,
Hi, I'm using a VSD and S7-1500 CPU with PROFINET connection. But the alarm occurs that there is not PROFINET connection when VSD power on. I guess that this cause is gap between PLC Startup time and VSD loading time. And press the ok button when plc loading time is finish. then VSD is showing "No failt / alarm is pending." I wish alarm is not occured. or remove the alarm message automatically like press the ok button.
Note, I was setting P1210 Automatic restart function parameter as 1. Acknowledge all faults without restarting.
Best Regards
Min Su Kang AttachmentScreenshots.zip (252 Downloads) |
Follow us on