1/3/2007 9:15 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello Julien Also a Happy New Year Perhaps you can use Report System Error. Here are some links: http://support.automation.siemens.com/WW/view/en/19378840 http://support.automation.siemens.com/WW/view/en/22319131 I hope it will help you. Best regards, Wizard |
1/3/2007 12:56 PM | |
Posts: 58 Rating: (1) |
[quote user="Wizard"]Hello Julien Also a Happy New Year Perhaps you can use Report System Error. Here are some links: http://support.automation.siemens.com/WW/view/en/19378840 http://support.automation.siemens.com/WW/view/en/22319131 I hope it will help you. Best regards, Wizard i have the error message system. BUT when the CPU is with a SF, for example if i take two modules of the ET200S, the CPU is in STOP and in SF ( In stop because there isn't the OB86). But in wincc flex, i don't have the message that the CPU is in SF But on the CPU the LED SF is lighted. Thanks Julien |
1/3/2007 1:46 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, when i understand you right, you want a message if the PLC are in "STOP". Did you know this FAQ => http://support.automation.siemens.com/WW/view/en/19687561 greetings, |
1/3/2007 6:30 PM | |
Posts: 58 Rating: (1) |
[quote user="The Brain"]Hi, when i understand you right, you want a message if the PLC are in "STOP". Did you know this FAQ => http://support.automation.siemens.com/WW/view/en/19687561 greetings, If the CPU is in stop I can displayed it in the alarm archive, because i work in integrated, so i displayed the S7 Message... But if the CPU is in System fault....i can't know it. More i'am looking for free solution. Thanks very much for your help Julien |
7/13/2015 3:41 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on