7/10/2015 4:32 PM | |
Joined: 10/10/2014 Last visit: 4/18/2024 Posts: 1725 Rating: (209) |
Hi jagang Do you have 2 redundant WinCC server or you have redundant PLC ? Best regards |
7/22/2015 7:53 AM | |
Joined: 1/21/2011 Last visit: 1/23/2024 Posts: 162 Rating: (1) |
Dear sir, I am using S7-300R PLC CPU319-3PN/DP & SCADA Wincc V7.0 Sp3. its is Software redundancy system & Scada i have created a single connection in TCP/IP driver. While trying for connection change over in the dynamic wizard. i have checked with new project with out OS project editor it is showing in the dynamic wizard please find the attached file for screen shot & kindly help me for connection change over between master & slave . Master PLC ipaddress: 192.168.0.1 Slave PLC ipaddress: 192.168.0.2 In scada i have created single connection with ipaddress of 192.168.0.1. Regards K.Jagan AttachmentError screen.rar (68 Downloads) |
Follow us on