8/11/2015 8:47 PM | |
Posts: 111 Rating: (1) |
I am modifying the machine and need modification in the program and I need to edit symbol let say bit I6.1 is "door open proximity" so I want to change the symbol "door open proximity" to "hydraulic" and keep the same address I6.1. When I right click on the contact and go to edit symbol it is not allowing me to edit symbol and the symbol is grey so what should I do to edit this as I want to edit one contact and want to apply on all the cross references in the program with the same address I6.1 Can anybody tell me what should I do here?
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/12/2015 11:03:26 AMNew subject after splitting |
|
Follow us on