3/20/2014 12:37 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating:
|
Hello, My suggestion would be checking difference in behavior of CPUs with different firmware version. As an example, check the following differences in behavior in a V6 CPU compared with a V4.5:
Consult with the Fault-Tolerant CPUs manual for changes in each newer versions. If you can not find the older manual, ask "support request" for assistance. Modify the old user program if itwill be effected by the change in firmware of new CPU.
|
3/28/2014 7:34 AM | |
Posts: 3 Rating:
|
Newer CPU with different order number. From 4HL04-5HT06.
|
3/30/2014 3:45 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating:
|
Hello, Personally, I think it is not possible to change a CPU from V4 to a V6 equivalent in a live process.To be sure, ask from here. Prior to that read section 17.2 for possible component changes for a Fault-Tolerant system HERE during operation. I hope it helps! Hamid Hosseini |
8/17/2015 10:42 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4769 Rating:
|
New question published by AutoGen_682437 is split to a separate thread with the subject Find 6ES7 417-4HL01-0AB0 CPU in TIA. Best regards |
Follow us on