8/22/2015 9:09 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
Thanks Christoph for you effords, I tried to make a configuration with TIA. I have CPU IM151-8F PN/DP, D435-2, TP1200 an PN/PN coupler. I have reserved 5 modules 4DO ET200S to be controlled by the D435-2. Classic way in Step7 was to export gsmdl file, when I tried to migrate to TIA I had to delete this I-device configuration, therefore I have tried to make a TIA configuration. If you look how is done in Step7 you will find a 4DO module with phsical address QB38 in I-device mode is named submodule1000 with address 258 (I address) and in my SCOUT configuration I have an output address PQB258. Whenever I set bits in PQB258 in D435 the ET200S outputs turns on/off. They are working in Step7. Since the TP1200 can be only programmed in TIA, I tried HMI_proxy but I would prefer to store and change entire project, I am afraid that when liking HMI_proxy again for new Step7 strored name, some bug will rise up. The only right direction would be to do everything under TIA, but I can't do the same configuration, TIA won't allow me to set address QB38, : this addres is already being used - of course it exists and I want to make an I-device from it. The next address what TIA proposes is Q43, which it doesn't exists physicaly. AttachmentForum_TIA_I-device.zip (164 Downloads) |
Follow us on