8/25/2015 10:34 AM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
hellow dear freinds, hope u guyz doing well, yes I am here with new query, it is as follows, I have winCC v7.0 sp2 ASIA, licensed RT AND RC, now I have exceeded the default limit of archived tags, could anybody suggest mi which licensed version for winCC archive will be compatible with version which I am using as mentioned above, Note: I have 700-800 tags to log and reporting. please suggest ASAP. thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/25/2015 1:32:53 PMNew subject after splitting Let's do it... |
|
8/25/2015 3:02 PM | |
Joined: 5/20/2015 Last visit: 4/29/2024 Posts: 216 Rating: (3) |
thank you sir, |
Let's do it... |
|
Follow us on