8/27/2015 3:51 AM | |
Posts: 305 Rating: (2) |
study an test the command of path ,but , have not machine to test the coordinate , via with CPU ,how can i test the command right or error ? |
8/27/2015 4:24 AM | |
Posts: 305 Rating: (2) |
thanks . but i want to know ,witch "var" ,can view the axis position ,and it about my control calcuate right or error ? |
8/27/2015 4:57 AM | |
Posts: 1529 Rating: (202) |
[Axis].positioningstate.actualposition should work for position feedback. It will always equal the reference, so following error will always be 0. |
8/27/2015 5:30 AM | |
Posts: 305 Rating: (2) |
no this var . wo want the var ,it can direct view coordinate positon , e.g. X-Y plane ,at the axis motion over ,the var view x or y coordinate position . |
8/27/2015 1:36 PM | |
Posts: 305 Rating: (2) |
ok,i just to read manual and find the command,has any problem ,i write it at this post 。 thanks。 |
Follow us on