8/27/2012 5:15 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (64) |
You can connect APL Structures to Shared DBs. You must create a STRUCT type in the DB and the elements of the Structure must match the APL Structure elements in Order, Name and Type. For the Pcs7AnIn block output parameter PV_Out has a structure of Value (Type REAL) and ST (Type Byte). Therefore, the Shared DB needs a STRUCT type with Value (Type REAL) and ST (Type Byte). See attached screen shot showing a Pcs7AnIn block connected directly to a shared DB. The Shared DB configuration is also shown for clarity cabreytj AttachmentC:\Documents and Settings\cabrtj\My Documents\My Pictures\PCS 7 V8.0 APL Structure to Shared DB.JPG (559 Downloads) |
Last edited by: cabreytj at: 8/27/2012 5:16 PM |
|
This contribution was helpful to1 thankful Users |
9/3/2015 1:27 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by nkr is split to a separate thread with the subject WinCC, radio button to single bool variable with structured variable. Best regards |
Follow us on