9/4/2015 11:21 AM | |
Joined: 1/28/2009 Last visit: 9/2/2024 Posts: 6846 Rating:
|
Dear User, In example M200.0 would have a same status as M100.5. It's a pointers I should use to make it work? Any advices? Using indirect addressing in STL will you all you need to perform such a task but you need more information regarding the absolute addresses, such a task can be easily done in SCL with indirect addressing.For more information ,I suggest the following source of information plus Online manual of STEP 7:
And the great source of information can be found in H.Berger "Automating With STEP 7 in STL and SCL".If you need our help, please explain more. I hope this helps, hdhosseini |
Last edited by: hdhosseini at: 9/4/2015 11:23:14 AM |
|
Follow us on