9/9/2015 3:59 PM | |
Posts: 27 Rating: (0) |
Hi, I try to connect with scalance X208 with IE. In documentation, i see: just write the ip adress on url, but what the default adress? Thanks all. François. |
9/9/2015 4:17 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308)
|
Hello There is no IP address preset from Factory. The initial assignment of an IP address for an Industrial Ethernet switch of the SCALANCE X-200 product line is not possible with Web Based Management because this configuration tool requires that an IP address is already available.
• DHCP Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
9/9/2015 4:19 PM | |
Posts: 27 Rating: (0) |
Many thanks for answers!!! |
Follow us on