9/14/2015 3:55 PM | |
Joined: 5/12/2006 Last visit: 6/4/2024 Posts: 22254 Rating: (2986) |
Hello, you can check it yourself in the compatibility chart: https://support.industry.siemens.com/cs/de/en/view/22611503 CP5512 is not compatible for Win7 x64. Other thing is that this CP Type will phased out in 10/2015, so no longer driver support. With TIA V13 SP1 you get a newer Version of the SIMATIC Device Drivers which remove the drivers from the system. You can open a support request with the topic "CP5512 driver for TIA V13 SP1" to get the drivers from the SIEMENS Support.
Christoph |
Follow us on