10/5/2015 9:38 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
I used another PC with OS = Windows 7 - Pro SP1 -x 64 Connected with Profinet and Simotion Scout v4.3.1.23 Regards, |
10/5/2015 10:01 AM | |
Joined: 5/12/2006 Last visit: 10/19/2024 Posts: 22422 Rating: (3023)
|
and which connection type you use? USS/PROFIBUS/PROFINET? |
10/5/2015 10:17 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
PROFINET Regards |
10/5/2015 10:50 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Yes , ping does work and also through ethernet node it's available. |
Follow us on