9/10/2009 7:27 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hello, About necessary cable check if your cable is like in Communication cable for Drive Monitor . Then conect cable, open Drive Monitor - Tools - Online Settings. There select Bus Type (USS) and Interface (COM1 9600 baud rate - Bus operation Automatic) Then open File - Set Up an USS online connection. There push start button. If you have connection with Drive, program automaticly will recognize the drive. Then just push open button and that's it. Hope this will helps. Best regards, Hristo Mihalev |
9/10/2009 8:05 PM | |
Posts: 8 Rating: (0) |
Thank you,it work great now i got all drive pra, again thank you |
9/11/2009 7:19 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Hello, You are wellcome! Glad to hear everything is OK now. Regards, Hristo Mihalev |
10/6/2015 11:42 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by ortsas is split to a separate thread with the subject Drive is still not detected in drivemonitor. Best regards |
Follow us on