11/12/2015 11:25 AM | |
Posts: 3 Rating: (0) |
Hi,I’m a beginner, and I’ve read all about - Sample program: S7-1200 and DATA LOG and data log help from all type of datalog blocks.I still don’t understand how the data log process does work.. :/ In my sample program I’m collecting temperature readings from my sensors and saving them in the datalog buffer as an array [0..4]. I would like to create a new file with eg. 1000 records on my MC and save the buffer every eg. 10sec-(using the timer from the Modbus rtu master). I would like to use the information’s “done” and “busy” to control the datalog process the same way like in the Modbus reading. But it doesn’t work.. I do not know what to do next. Could You look at my sample program and could I get from You some advices how to solve my problems?
I’m using Version V11 SP2 Update 5. best regards ------------------------------------------------------------------------------------------ AttachmentMODBUS_RTU_MASTER.rar (112 Downloads) |
Last edited by: Min_Moderator at: 11/12/2015 3:11:04 PMNew subject after splitting |
|
Follow us on