11/13/2015 12:30 PM | |
Posts: 223 Rating: (0) |
Hello all :) I 've got this script to print reports per ended batch (see attachment). This script is triggered when the productorder is changed. Also on the report, I want to print the productorder that just has ended (so the old value). So every time a report is printed, I copy the new vaue of the productorder (in which the productorder has just changed) to a backup internal tag. (this is the last 2 lines in the script). In that case, when the script is once again called, the previous value is printed. At least that's what I want to do. But when I test this, the new value is printed. In the meantime I'v noticed that printing the report itself takes around 3 seconds. Could it be that while printing, executing of the script continues and thus the new value is printed? If yes, how do I work around my problem? Any suggestions? Thanks in advance. AttachmentReport_Print.doc (122 Downloads) |
Follow us on