8/1/2011 11:04 AM | |
Posts: 49 Rating:
|
Hi Where can i download Service Pack 2 or Service Pack 3 for PCS7 v7.1? How can i update PCS7 v 7.1 SP1 to SP2? |
8/1/2011 11:28 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating:
|
Hi HSCD, Have a look on the SIMATIC PCS 7 V7.1 + SP3 Released for Delivery http://support.automation.siemens.com/WW/view/en/50721458 (The L price for the SIMATIC PCS 7 Software Media Packages is 50,00€ in each case. The L price for the SIMATIC PCS 7 Update Package Engineering V7.1 + SP1 to V7.1 + SP2 is 25,00 €. Please note that additional freight and customs charges may become applicable.) You will Find the information in the Above link. Information and brief instructions for updating/upgrading PCS 7 software |
Ammy |
|
12/10/2015 11:58 AM | |
Joined: 9/30/2015 Last visit: 9/7/2022 Posts: 23 Rating:
|
where can i down load pcs7 v7.1 |
12/10/2015 1:31 PM | |
Posts: 567 Rating:
|
Hi rachnaarul, PCS 7 is not avaiable as download. You have to contact your regional Siemens Contact/Partner. You can find the contact under the following link: |
This contribution was helpful to
1 thankful Users |
Follow us on