5/2/2012 4:59 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1165) |
Hello Trimmer, Have you seen this link: What settings do you have to make on an MP377 to reset the operator panel to the factory settings? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
5/2/2012 6:02 PM | |||||||||
Joined: 5/28/2008 Last visit: 7/4/2024 Posts: 4510 Rating: (837) |
Hello, Please tell me did you checked that you have entered the MAC address correctly? Please check that you have made the procedures as instructed in this link: And also have a look on this link: Hope this helsp.
|
||||||||
Last edited by: Ayman Elotaify at: 5/2/2012 6:05 PMSorry... I have just noticed that Wizard have put the same link. Ayman Elotaify |
|||||||||
5/2/2012 7:19 PM | |
Posts: 559 Rating: (87) |
Dear Trimmer, Once u complete the procedure which is mentioned in above posts. You just connect Ethernet switch between HMI & PC. Surely you will get connection. |
5/3/2012 12:12 PM | |
Posts: 2 Rating: (0) |
This seems to be the missing link. Thanks for all of your responses. |
This contribution was helpful to2 thankful Users |
1/11/2016 3:32 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by BT123456789 is split to a separate thread with the subject Upgrade OS on MP377 from 2007 to WINCC Flexiable 2008, Error. Best regards |
Follow us on