1/2/2015 8:21 PM | |
Posts: 1 Rating: (0) |
I am also having an issue communicating between a S7-200 and S7-1200. In the S7-200 PLC's wizard I have a client connection selected which is my third connection.The local TSAP is set to 12.04 ( which this number is auto generated.)The remote TSAP I have is 03.00 and I have my IP address set to 10.12.122.106 which is the IP address of my 7-1200 processor. I have the enable the keep live connection checked. The S7-1200 processor is the only module for that rack. There is no reference to the S7-1200 as an option. I have tried setting it up for the 10.00 for the remote TSAP, but then the channel never gets to the ready state. When I have it set to 03.00 the channel is in the ready state, but I get the error 6. --------- New subject after splitting from connection S7-200 & S7-1200 via Ethernet. |
Last edited by: Min_Moderator at: 1/5/2015 5:36 PMSplitted |
|
1/30/2015 10:51 AM | |
Posts: 267 Rating: (22) |
Hello, do you know this: http://support.automation.siemens.com/WW/view/en/40622389 |
1/12/2016 9:34 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by velvetx is split to a separate thread with the subject Connection between S7-1200 and S7-200 with CP243. Best regards |
Follow us on