4/16/2011 7:51 AM | |
Posts: 691 Rating: (37) |
I am having problem in communicating CP341 as Modbus Master. In the First TIme I was able to establish communication with the Slave and the CP341 and got error related to illegal Data Querry. Then I executed Reset parameter of the Modbus FB(P_SND_RK). after that I am getting continuous error code (1E0F), which is related to CP341. I tried to overcome this problem by recycling the power of the CP , changing the CP; but got the same same error code. I am not able to understand the error code. Does anybody have any idea regarding this? Splitted from Problem using CP341 with Modbus Master. |
Last edited by: O_Moderator at: 4/18/2011 8:26 AMnew subject after splitting |
|
2/3/2016 1:30 PM | |
Posts: 6 Rating: (0) |
Niranjan Have you solved the problem? |
Follow us on