2/17/2016 6:57 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello saravanan; This manual should have all the information and instructions required to connect your CPU to Modbus/TCP using a CP 343-1. SIMATIC Modbus/TCP communication using CP 343-1 and CP 443-1 https://support.industry.siemens.com/cs/ww/en/view/103447617 The attached screenshot shows the required license (yes, this is not a free download) and the FBs that are used to program the exchanges. Note that there is a free demo software available, but your PLC will run with diagnostic LEDs until the license is properly installed. For test purposes it is sufficient, see the following FAQ: How do you establish OPEN MODBUS / TCP communication from a SIMATIC S7 and where can you find further information? https://support.industry.siemens.com/cs/ww/en/view/22660304
Hope this helps, Daniel Chartier |
Follow us on