2/20/2016 9:34 AM | |
Posts: 163 Rating:
|
Hello, I tried this CFC and got this issue upon Compilation. |
2/23/2016 7:52 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hello Idir, In your compilation log, I see that you are using a CPU 414-3. I'm curious which PCS7 you use? Maybe the CPU is not supported like in the released modules-manual. Is your test project migrated from another version? Do you have problems with others blocks? What you can do is checking your blocks in the project. For this, do the following: 1. In CFC editor, go to Options->Block Types 2. Select all blocks in the "Chart folder" (Right-side). 3. Now press: "New version...". The complete CFC charts are checked to make sure the blocks folder (offline program) are equal to the blocks used in CFC. 4. Try a new compile after doing the above. Another thing you can do is to delete all the system charts in the "Chart" folder. The system charts start with "@". Only delete those!! The compile will generate the system charts again when Generate module drivers option is selected during the compile of the program. Please let me know if this helped, or if you received error messages. |
Last edited by: Oreca at: 2/23/2016 7:53:33 PMLast edited by: Oreca at: 2/23/2016 7:57:15 PMIf I could help you, you can use the RATE button. Thank you. |
|
2/24/2016 9:50 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hello Idir, To addition of the comment from mark, sometimes a newer firmware is needed for the CPU in order to work with a newer version. If you open hardware configuration, you can select a profile for the choice of components on the right side. If the profile is set to "PCS7_V81", then you can select CPU's which are released for 8.1. I don't know which firmware you have...The 414 you list is supported with firmware v3.1. Having a MMC card does not matter whether or not it is supported in PCS7 8.1 PS: OB88 not loaded normally means a programming error. Can you check some diagnostics? |
Last edited by: Oreca at: 2/24/2016 10:01:28 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on