2/26/2016 7:17 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Hello MD_dx, So just to be clear, you have a Siwarex and simocode block inserted in your project, but on WinCC you cannot open the faceplate? Or do you mean that the block icon for the blocks are not created? If you cannot open the faceplate, but you have a block icon, then do the following: 1. In WinCC runtime, go to C:/Program Files (x86)/SIEMENS/WinCC/uTools and then execute: "apdiag.exe". It is a tool to check errors in scripting. 2. When opened, click on "Output Window" and then on "Open". 3. Click on the block icon of the siwarex and then on simocode. 4. Post back the errors you'll get. I think when you cannot open the faceplate, the name of the faceplate is not correct, or something is missing. If the issue is not the faceplate but the block icon, please let me know. |
If I could help you, you can use the RATE button. Thank you. |
|
2/26/2016 9:43 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Well, I hope I understand your post: If you want to show the faceplates on a client, you have to copy all faceplate (.pdl) to the client as well in the GraCs folder of the client project. I'll answer for mark, it's no difficult procedure . On the OS server or client, in WinCC explorer, you can select "OS project editor" In there you have several options: 1. You can choose the layout for your PC. In case of a client you can select one, two, four screens with specific resolution. 2. You can select system messages to display, how many faceplate can be opened at the same time etc. 3. You can configure the Picture Tree, change area's, 4. Define if changed pictures/emf files needed for display of OS objects are changed back to project settings or not. It is basically the configuration of your OS. |
If I could help you, you can use the RATE button. Thank you. |
|
2/26/2016 1:08 PM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Hi Mark, Your're right about the additional scripts and such. But it's still not clear what the exact issue is. MD_dx has to send us more info I quess.. |
If I could help you, you can use the RATE button. Thank you. |
|
2/27/2016 3:40 AM | |
Posts: 70 Rating: (0) |
I solved my problem with "OS Editor" Thank you both. I rated for those post. :D |
This contribution was helpful to2 thankful Users |
2/27/2016 5:21 PM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928) |
Thank you! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on