(0)| 1/5/2008 1:51 AM | |
|
Posts: 2 Rating:
|
Hi Sfestiva Please, tell me what modification, because i can whit nubitek, but with the other, i can't |
| 2/22/2008 8:30 PM | |
|
Joined: 9/29/2005 Last visit: 12/2/2025 Posts: 313 Rating:
|
Hi partypeople, i can feel with you when you are sad about MAS5. The big challence was there to make it possible to use TC65 Terminal, MD720-3, TC35i/T and maybe MC45. Normally the AT module should be comatible to each other module. but it isn´t. Especially the MD720-3 has no direct connection to the gsm module but only a AT compatibility mode..... Also a lot of differences regarding the countries (prefix messageservicecentral, response timings after GSM login....) was a big challenge. I think with the most actual version of MAS5 library which came out this week, everything should work without problem. And please notice:(!!!!) When you have problems. Post it. MAS_Forum The last library update was made together with some guys from the german forum. When you have problems or ideas post it and you will maybe see your suggestions in the next version. hmmmm i must try the library from nubitek |
| 3/6/2008 12:53 PM | |
|
Posts: 8 Rating:
|
Hi Lifrasil: The communication libraries of Nubitek can be downloaded and tested for free. Visit the site www.nubitek.com where you can access the software and corresponding documentation and samples. Regards, Lorenzo |
Follow us on