3/11/2016 2:34 AM | |
Posts: 6 Rating: (0) |
Hi experts, I am trying to connect to sinumerik sinamics drives with Sinamics Scout 4.4 but no success connecting to drives at NX15 modules. I am connecting to 192.168.214.1 network at NCU 720 I was able to go online with step7 and interface works OK. See attachment for details. only difference I see between drive unit 1 and Sinumerik integrated DP that they are on a DP network. Not sure why I cant get in to drives at NX modules Thanks in advance AttachmentSiemens Pics.zip (92 Downloads) |
3/13/2016 6:36 PM | |
Posts: 6 Rating: (0) |
Thanks, Here is all the info. I am attaching the project file also AttachmentDesktop.zip (97 Downloads) |
3/13/2016 6:52 PM | |
Posts: 6 Rating: (0) |
Here is the project file I had to split it copy all files in to main folder |
Last edited by: AutoGen_63091 at: 3/13/2016 8:32:34 PM |
|
3/13/2016 6:54 PM | |
Posts: 6 Rating: (0) |
Second folder
Attachmentcopy these to main folder.zip (96 Downloads) |
3/13/2016 6:55 PM | |
Posts: 6 Rating: (0) |
Third folder
AttachmentCopy file to main folder.zip (80 Downloads) |
3/13/2016 7:07 PM | |
Posts: 6 Rating: (0) |
I am trying to connect the port X136 MPI/DP with CP5711 adapter. Set the laptop pg/pc to CP5711 profibus |
Follow us on