4/7/2016 7:25 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
So you mean "Retrieving" the project.. Can you tell me why you cannot? Do you get errors? Also, please list the PCS7 version you are working on. And to addition: On which PCS7 version do you want to retrieve the project? |
If I could help you, you can use the RATE button. Thank you. |
|
4/7/2016 7:50 AM | |
Joined: 9/16/2013 Last visit: 4/24/2024 Posts: 199 Rating: (23) |
you could try to unarchive your project with a standard zip program. |
4/8/2016 7:14 AM | |
Joined: 8/25/2006 Last visit: 5/12/2024 Posts: 2203 Rating: (277) |
Hello. Did you try to select another path for archiving (not the Desktop)? |
4/8/2016 7:31 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hi Nachate, You can try a few things: - Does the project folder have the "Read only" attribute (right click the project directory)? - You can try to do a "Save as, with reorganization (slow)" in order to restore gaps and align project settings. Select the multiproject and in Simatic Manager -> Save as... |
If I could help you, you can use the RATE button. Thank you. |
|
4/8/2016 2:00 PM | |
Joined: 11/29/2011 Last visit: 5/7/2024 Posts: 1358 Rating: (230) |
Hi, This article discuss your problem: What remedies are available when it is not possible to archive or retrieve STEP 7 projects? |
- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to2 thankful Users |
Follow us on