4/16/2016 10:06 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Unfortunately all changes made in CFC are directly changed in the database, there is no save,undo and redo option, not even in later versions.. When I need to take a look at the program to check or change a vakue, when I open CFC or SFC, I always enable test mode right away..changing is not possible. In later versions, you can also enable write protection for charts (under Chart folder) so you cannot change anything |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on