4/21/2016 2:42 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello Ayman yes you are right the SP3 itself you cannot download. But the Link of User Wizard is the correct one. The SP3 for WinCC flexible 2008 ist not available standalone. Its only a full installatoin of !WinCC flexible 2008 incl SP3! so if you have a Licence for 2008 you can work with the Installation of the Link https://support.industry.siemens.com/cs/ww/en/view/100777999 Siemens confirmed to me that its the Full Installation Medium that you have also on DVD. Bye Murof |
Last edited by: The Helping Hand at: 4/21/2016 3:11:35 PMMade the link clickable. If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on