4/20/2016 3:32 PM | |
Joined: 3/14/2008 Last visit: 8/9/2024 Posts: 2081 Rating:
|
Hi, Do you have a screenshot of the CTU block how you configured this in CFC? It should be no problem to operate this block. There are two versions: FB24 from the CFC library and SFB0 from the standard library. Make sure you use FB24. The FB24 is available in two versions also: CFC library->ELEM_300 (for CPU300) or ELEM_400 (for CPU400). Make sure you have the correct version which is ELEM_400. PS: ELEM_400 is the author name which can be accessed from the block properties in CFC. It works both, but better use the block designed for CPU400. Maybe there is something else wrong like the runtime group which is disabled, or the pulse input is in a different OB where cycle problems can occur. |
If I could help you, you can use the RATE button. Thank you. |
|
4/21/2016 1:03 AM | |
Posts: 5 Rating:
|
Hi You are right, i used CTU from ELEM_400, thanks a lot for your help.
|
4/21/2016 7:51 AM | |
Joined: 3/14/2008 Last visit: 8/9/2024 Posts: 2081 Rating:
|
Hi Omars7, Glad to help!! But is your problem solved now?? |
If I could help you, you can use the RATE button. Thank you. |
|
4/23/2016 1:46 PM | |
Posts: 5 Rating:
|
Hi, Sorry to be late, the problem is solved by choosing a CTU block from ELEM_400, thank you very much. |
4/23/2016 7:01 PM |
|
Joined: 3/14/2008 Last visit: 8/9/2024 Posts: 2081 Rating:
|
Hi Omars7, OK, good to hear! Glad I was able to help you. Have a nice weekend. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on