4/18/2016 9:10 AM | |
Joined: 5/28/2008 Last visit: 9/5/2024 Posts: 4515 Rating:
|
Dear Hristo, I agree with Mr. H-H to start a support request immediatly. When I faced this problem few years ago, I started a support request. They then send to me this tool called (S7-DUMP) And asked me several questions (Bellow all of these questions) S7-DUMP is an internal tool which can communicate with the CPU and get some data from the CPU. The output file can not be read from me. So, I am sure that there is another tool they have in Siemens to decode the output file of S7-Dump. Attached also instruction of this tool. If you have a similar problem you should start support request and they may give you this tool and then you will send them the output file. They will decode it and give you the results. That's all. Questions I recieved from the support was as follows:
AttachmentAnleitung_Werkzeug_S7Dump_ab_V5-und_V4.5H-CPUs.pdf (425 Downloads) |
Ayman Elotaify |
|
Follow us on