4/28/2016 12:10 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi Berg, I don't know your system setup. Maybe you can show us? But I'm pointing you to my attachment. I have collected some diagnostic documents for you to check. I don't know your specific setup, but with the help of the documents, you can narrow down your search. I think they are very useful. Further, I have one big document which i'll upload. It's too big for here. See end of this post. There could be a lot of things, also easy checkmarks like the setting: "Default Master" in the redundancy settings of the OS servers. The OS standby must have this checkbox cleared. If you also check it, problems could occur. It could be related to NetPro configuration (Named Connections-Station Configurator-Configured/PG mode of the network card). A lot of things could go wrong... AttachmentDiagnose.zip (72 Downloads) |
Last edited by: Oreca at: 4/28/2016 12:14:19 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
4/29/2016 8:37 AM | |
Posts: 56 Rating:
|
Hello Berg, You can also check with the help of Wincc< channel dignosis in OS whether the tags are connected or not to with this tool. Thanks, Ashish |
Follow us on